AXIS#.WS.NUMLOOPS

Description

This parameter sets the maximum number of wake and shake repetitions. AXIS#.MOTOR.PHASE is calculated as mean value of all wake and shake repetitions.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

counts

Range

0 to 20 counts

Default Value

5 counts
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
AXIS1.WS.NUMLOOPS

5013h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.WS.NUMLOOPS

5113h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.NUMLOOPS

6705

1A31

Unsigned8

Read/Write

-

AXIS2.WS.NUMLOOPS

72241

11A3

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.NUMLOOPS

6705

Unsigned8

Read/Write

-